NXP Semiconductors logo
LPCXpresso Logo

Reply
 
Thread Tools
  #1  
Old 08-06-2012, 11:15 AM
il_mix il_mix is offline
Junior Member
 
Join Date: May 2012
Location: Italy
Posts: 4
il_mix is on a distinguished road
Default "No emulators" error

Hi everyone.
I'm using a custom board with a LPC1788 and a LPC1313 on it. I'm used to program both using LPCLink on LPCXpresso board.
I'm using WindowsXP and LPCXpresso v4.2.0 [Build 264] [24/02/2012].
Everything worked fine since a while ago...

I get a strange error now when trying to program the LPC1313, that seems to be connected more on the IDE than on the hardware.
When I try to program the LPC1313, or erase its memory, I get a "No emulators" error.

I noticed that when trying to erase LPC1788 memory (after setting LPC1788 in "MCU settings"), with the MCU disconnected from the LCPLink, the IDE think about it a little, than give me:
"02: Failed on connect: Ep(01). Target marked as no debuggable.".
With LPCLink connected, the MCU erase/programs correctly.

When I try to erase memory of LPC1313 (after setting LPC1313 in "MCU settings"), again with LPCLink disconnected, I get a "No emulators" error as soon as I start the erase process.
I get the same error with the LPCLink connected.

What's going on?
Thanks for your help!
Reply With Quote
  #2  
Old 08-07-2012, 10:16 AM
il_mix il_mix is offline
Junior Member
 
Join Date: May 2012
Location: Italy
Posts: 4
il_mix is on a distinguished road
Default

After reinstalling LPCXpresso the error is gone.
Don't know what happened...
Reply With Quote
Reply

Thread Tools

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is Off

Forum Jump



All times are GMT +2. The time now is 04:23 AM.