NXP Semiconductors logo
LPCXpresso Logo

Reply
 
Thread Tools
  #1  
Old 03-06-2010, 03:33 AM
rmteo rmteo is offline
Senior Member
 
Join Date: Feb 2010
Location: USA
Posts: 126
rmteo is on a distinguished road
Default LPCXpresso Base Board

Anyone have the LPCXpresso Base Board as mentioned here http://knowledgebase.nxp.com/showthread.php?t=5

What do you think of it?
Reply With Quote
  #2  
Old 03-06-2010, 07:20 PM
brucesegal brucesegal is offline
Member
 
Join Date: Feb 2010
Location: canada
Posts: 41
brucesegal is on a distinguished road
Default

I have one. Nice board as it allows you to exercise all the peripherals without a lot of effort. It all depends on what you are trying to accomplish.
Reply With Quote
  #3  
Old 03-08-2010, 04:27 PM
rmteo rmteo is offline
Senior Member
 
Join Date: Feb 2010
Location: USA
Posts: 126
rmteo is on a distinguished road
Default

Thanks. I have one as well. Really nice and great value (like the LPCXpresso tool chain) at $99. The included routines/drivers are a great help in understanding the workings of the LPC1xxx. Does anyone know of a compatible target board with a LPC17xx besides the MBED?

Reply With Quote
  #4  
Old 03-08-2010, 04:51 PM
renan renan is offline
Senior Member
 
Join Date: Dec 2009
Location: Porto Alegre
Posts: 145
renan is on a distinguished road
Default

Quote:
Originally Posted by rmteo View Post
Does anyone know of a compatible target board with a LPC17xx besides the MBED?
That's something I would like to know.

Renan
__________________
http://renbs.blogspot.com
Reply With Quote
  #5  
Old 03-08-2010, 10:19 PM
rmteo rmteo is offline
Senior Member
 
Join Date: Feb 2010
Location: USA
Posts: 126
rmteo is on a distinguished road
Default

Quote:
Originally Posted by renan View Post
That's something I would like to know.

Renan
Send EA an e-mail. They may have interesting info for you.
Reply With Quote
  #6  
Old 03-09-2010, 04:00 PM
NXP_Europe's Avatar
NXP_Europe NXP_Europe is offline
Support Team member
 
Join Date: Dec 2009
Location: Nijmegen, The Netherlands
Posts: 324
NXP_Europe is on a distinguished road
Default LPCXpresso Base Board

Hi All,
Besides mBed there are no pin compatible LPC1700 boards for the EA Base board yet. We're working hard on a LPC1700 LPCXpresso. So that one you can expect soon.


Kind regards,
__________________
- NXP European team -
Reply With Quote
  #7  
Old 03-09-2010, 04:15 PM
rmteo rmteo is offline
Senior Member
 
Join Date: Feb 2010
Location: USA
Posts: 126
rmteo is on a distinguished road
Default

Quote:
Originally Posted by NXP_Europe View Post
Hi All,
Besides mBed there are no pin compatible LPC1700 boards for the EA Base board yet. We're working hard on a LPC1700 LPCXpresso. So that one you can expect soon.

Kind regards,
Thanks, NXP_E. That is what the hardware people told me as well.
Reply With Quote
  #8  
Old 03-11-2010, 04:35 PM
bladerunner bladerunner is offline
Junior Member
 
Join Date: Nov 2009
Location: UK
Posts: 5
bladerunner is on a distinguished road
Default

Quote:
Originally Posted by rmteo View Post
Anyone have the LPCXpresso Base Board as mentioned here http://knowledgebase.nxp.com/showthread.php?t=5

What do you think of it?
Have the base board and LPC1114 module. It's good value, especially considering the entire toolchain (HW + Code Red IDE / compiler). And the lot work together nicely. As mentioned the code example's are useful to get up and running.
Recommended
Reply With Quote
  #9  
Old 03-25-2010, 07:27 PM
caprock caprock is offline
Member
 
Join Date: Mar 2010
Location: Calif, USA
Posts: 80
caprock is on a distinguished road
Default have mbed & base board

I have the mbed 1768 and the lpcexpresso base board Rev A but do not have the 1114 board.

This combination seems to be a good debug/develop platform except for the fact that I can't seem to extract the sample programs without first setting up the code red IDE, which seems to entail that the lpcxpresso 1114 board is required as well.

Does anyone have a suggestion as to how to extract the source code that seems to be embedded in the projects? At the moment I was trying to get the 'Shift Reg to 7-Segment' section to work from the mbed, and would really like to see the simple driver code.

Thanks
Reply With Quote
  #10  
Old 03-25-2010, 07:58 PM
rmteo rmteo is offline
Senior Member
 
Join Date: Feb 2010
Location: USA
Posts: 126
rmteo is on a distinguished road
Default

Quote:
Originally Posted by caprock View Post
...This combination seems to be a good debug/develop platform except for the fact that I can't seem to extract the sample programs without first setting up the code red IDE, which seems to entail that the lpcxpresso 1114 board is required as well.

Thanks
You don't need the LPCXpresso 1114 board to extract the examples using the Code Red IDE if you do not intend to do any debugging.
Reply With Quote
Reply

Thread Tools

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is Off

Forum Jump



All times are GMT +2. The time now is 12:31 AM.